This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC2564: CC2564MODN

Part Number: CC2564

Tool/software: Code Composer Studio

Hi all,

I'm trying to set up CC2564 module into FCC testing mode. 

I'm using VS_Enable_FCC_Test_Mode function provided by Bluetopia which allows me to set proper modulation type, power level, channel, etc. 

This works just fine, functions return 0 and transmits  for a short period of time after which RF signal is turned off.

I set a while loop immediately after the function call.

Me question is either the VS_Enable_FCC_Test_Mode shouldn't set the module in continuous transmit mode intend of turning it off?

Thanks,