Other Parts Discussed in Thread: AM3358, , , CC2564
Tool/software: Linux
Hardware:
Beaglebone Black-Rev C (AM3358)
Boost-cc2564moda
Interface:
Beaglebone black Boost cc2564moda
UART1_Tx -----------------------------BURX1
UART1_RX -----------------------------BUTX1
UART1_CTSN--------------------------BURT1
UART1_RTSN--------------------------BUCT1
GPIO_44 ---------------------------------BnSD1
DGND ------------------------------------GND
image used:
root@beaglebone-yocto:/lib/firmware# uname -a
Linux beaglebone-yocto 4.15.13-yocto-standard (custom build)
While executing the demo application i am getting the below error.
root@beaglebone-yocto:~/CC2564/bin# ./SS1
Error:
PBAM>1 1
BTPM_Initialize() Success: 0.
DEVM_RegisterEventCallback() Success: 5.
PBAM>9 1
echo 44 > /sys/class/gpio/export
sh: line 0: echo: write error: Device or resource busy
echo out > /sys/class/gpio/gpio44/direction
echo 0 > /sys/class/gpio/gpio44/value
echo 1 > /sys/class/gpio/gpio44/value
echo 0 > /sys/class/gpio/gpio44/value
echo 1 > /sys/class/gpio/gpio44/value
BT COMM PORT (/dev/ttyO1): 1
Status: Executing BTS Script /lib/firmware/TIInit_6.7.16.bts.
Error: Could not open the script file /lib/firmware/TIInit_6.7.16.bts.
echo 0 > /sys/class/gpio/gpio44/value
DEVM_PowerOnDevice() Failure: -4, Unknown Error.
Function Error.
PBAM>quit
The bts TIInit_6.7.16.bts file is already in /lib/firmware . How to solve the above mentioned issue .