Other Parts Discussed in Thread: BOOSTXL-CC2650MA, CC2650
Hi,
Can the CC2650MODA be programmed using UART?
Regards,
Ajith
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Can the CC2650MODA be programmed using UART?
Regards,
Ajith
Follow to generate a .out or .hex file for the project you want to flash into MODA. Then you open flash programmer 2.
and select CC2650 in the list marked with an arrow. Right click on the selected device (where it's marked with unknown in the picture above, this will change to CC2650) and select connect. Then you can flash the image.
Note that the resistor in the schematic is external to the module
Ref 7.2.1 in the datasheet: "The reset line should have an external pullup resistor unless the line is actively driven. Placement of this component is not critical"