Tool/software: TI-RTOS
Hi TI,
Device |
CC2640R2LAUNCHXL |
SDK |
simplelink_cc2640r2_sdk_2_40_00_32 |
IDE |
IAR8.20.2 |
Reference Project |
Multirole |
We have custom FOTA process in our application. FOTA image will be stored in external flash. After completion, we are verifying the downloaded image and doing soft reset HAL_SYSTEM_RESET();
We have seen the halt in bootloader issues with below steps.
- Flashing from JTAG.
- No power reset to the board.
- Download FOTA image.
- Upon completion of download Call HAL_SYSTEM_RESET();
- Jumps to boot loader to update the software in internal flash.
- But halts in boot loader and will not update the flash/firmware.
But if we do the power reset after the flash it boots up properly.
What could be the issue?
Thanks
Niranjan Hegde