This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2538-CC2592EM-RD: 38MHz crystal or TCXO recommendations for outdoor extreme temp application

Part Number: CC2538-CC2592EM-RD

My customer is developing a system based on CC2538-CC2592EM-RD. The system will be exposed to extreme temperatures (-40C to 50C). We are looking for crystal or TCXO recommendations that will maintain high accuracy under these conditions. 

  • Have you checked the xtals that are used in the BOM for http://www.ti.com/tool/CC2538-CC2592EM-RD?

    Note that most commercial components are rated from -40 to 85 degrees C. You are not stating what "high accuracy" mean.  

  • Thanks for the reply. The customer is making several H/W changes to improve RF robustness. They are looking for 32MHz clock options that offer lower than 20ppm stability / 10ppm tolerance and that spec the frequency down to -40C. The crystal used in the CC2538-CC2592 reference design only specifies the frequency tolerance down to -20C. The customer is willing to move to a TCXO and they are asking if TI has any recommendations. 

    I just noticed that the title incorrectly states 38MHz. This was a typo as the design actually requires 32MHz. I am unable to edit the title.

  • For some reason I assumed that the xtal used in the ref design had the same temp spec as the chip.

    I could not find any other recommendations than the one used in the ref design. I would recommend contacting the xtal manufacturers directly and provide them with the wanted spec, including the spec that is given in the "32-MHz Crystal Oscillator" table in the datasheet. It also look like it exist different variants of the xtal used in the EVM BOM with larger temp range: https://www.digikey.de/product-detail/en/epson/FA-128-32.0000MF20X-K5/SER4079TR-ND/5209190 (I haven't checked all parameters towards the datasheet. I just used the filtering to come up with some options)