Part Number: CC256XSTBTBLESW
Hello,
I am working with the following system: STM3240G-EVAL Board + CC256XEM-STADAPT Board + CC2564MODNEM Board and I am exploring the CC256XSTBTBLESW.
I am experimenting both the HSP and the HFP demo and I have some questions:
- it should be possible to modify the example so that the controller does not decode the audio and instead send it to the host? What modifications are needed?
- for the HFP demo, it should be possible to disable the 16 kHz feature, in order to develop an HFP + LE application?
Thank you,
regards
Arianna