|
Device |
CC2640R2LAUNCHXL |
|
SDK |
simplelink_cc2640r2_sdk_4_20_00_04 |
|
IDE |
IAR8.32.2 |
|
Reference Project |
Multirole |
Hi Ti,
We have updated a custom procedure on GAP_LINK_ESTABLISHED_EVENT. Connected device will be verified by some data exchange. To keep it inline we are Pausing the advertisement on the link establish event. Then Resuming the advertisement after the device identification is done.
Here I have added the simplified the procedure.
Problem statement
- We have used mobile phones (BLE 4.1 and above) and other CC2640R2F devices for connection. In these cases everything is working fine.
- But with two “BLED112” (BLE4.0) device connected our CC2640R2F stops advertising. (always)
- And advertise starts after disconnecting one of the “BLED112” device.
- This has been observed using packet sniffer also.
- We also observed that, if advertisement is not paused after the link established event, the repetition of issue is lesser.
Questions
- What could be the reason? What could have gone wrong here?
- Will advertisement stops on normal connection event ?
- What are the parameters we can check and debug?
Thanks
Niranjan Hegde