Other Parts Discussed in Thread: TRF7970A
Hi I am designing an NFC Tag Reader and Writer CIrcuit that should be able to Read and Write NFC Tags of tag2 Type. In my System, the host controller (ATTINY1617) will interface with the TRF7964A over
SPI Bus, from the Data Sheet I am not able to understand the functionality of the
MOD PIN- Do I need to connect to the Host controller or can simply be pulled down to GND by some 10K resistor, I saw in some reference circuit they are pulling it down to GND
SYS_CLK : My Host controller has it own clock, do I need to connect the SYS_CLK to the Host controller, if not should I leave it floating or PULL to VI or GND
ASK/OOK - DO I need to connect this pin to the HOST controller.
Any help will be appreciated. Look forward for support
Thanks & Regards
Orvi