Other Parts Discussed in Thread: TLV61225, RF430CL330H
Hello,
I'd like to use the RF430FRL152H for an implantable application and I'd like to power a high current device that can pull up to 20 mA instantaneous current and up to 5mA DC current from VDD2X. Would that be a problem for this IC? What is the maximum current capacity of the VDD2X pin. Does VDDSW/VDDB have more current capacity? I'm also planning on using a boost converter to bump the voltage from 1.5 (or 2.9) to 10V do you foresee any issues by doing this with that chip?
That's all.
Thanks!