Hi Team,
According to the official reference, could I rewrite the ADC in RF430FRL152HEVM, remove R16 at SV16, connect the third hole, which connects ADC0 to SV16, with an external k thermocouple analog sensor? In this way, without changing any other parameters, could I use the GUI to achieve the purpose of measuring temperature? K thermocouple output voltage is 0-65mV, and I wonder if I still need another amplifier circuit?
The thermocouple converts a temperature signal into a voltage signal with an amplitude range of 0-60mV. Could I directly remove R16 from the evaluation board, and then connect a thermocouple and an instrumentation amplifier to the ADC0 interface of SV16 for temperature measurement, and use the official GUI for wireless temperature measurement?
Kind regards,
Katherine