Hello,
I want to measure voltage at a given point by two or more ADCs of CC2510. Please refer below intended circuit diagram
I am using P0_2 line for reading the ADC. If only one CC2510 is connected, the readings are correct. When I connect two or more, the voltage on the line is going equal to Vcc. Please help.
I have also observed, if a single CC2510 device is connected, during conversion process, there is a true voltage on the line. Once the conversion is complete, the line voltage goes to Vcc. How to resolve this?