This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TRF7970A: An “ISO15693 ROM Sensor Support Disabled” Error has occurred when RF430FRL15XH GUI Interface tring to request temprature of RF430FRL152H Patch in 'Demo Mode'

Part Number: TRF7970A
Other Parts Discussed in Thread: RF430FRL152H,

Hello,

  As the title suggests, when I try to use the RF430FRL15XH GUI Interface Version 1.3.1.0 to read the ADC2 pin in my RF430FRL152H Patch, which is connected to a 100k thermistor, the GUI reports an error "ISO15693 ROM Sensor Support Disabled" as below. The GUI works in Demo Mode mode and the issue is not resolved after I click "Yes" either. I'd like to ask if I need to do any other specific setup. What perhaps caused this to happen? Or is there a guide that you can provide for me? Please help me, thank you very much!

  

Best regards,

szx