Hello everyone,
in an investigation it was examined whether the TRF7970 is correctly controlled via SPI, it at his point it seems to be good.
By Checking the Datasheet (Version: SLOS743B - August 2011 - Revised March 2012) describes the SPI Mode for writing with SPI in Mode 0 and Read SPI in Mode 1. The Datasheet in Version: SLOS743M – AUGUST 2011 –REVISED MARCH 2020 describes SPI MODE 1 for writing and reading. (see attached image). The linux kernel driver implements for writing and reading mode 1, this behavior was confirmed on the SPI Bus.
My Questions:
- Are there several silicon versions with different behavior of the chip's SPI modes on market?
- or is the "old" Datasheet completely wrong (see link above of the compared datasheets).
Thanks a lot for your help