Part Number: CC2530
Other Parts Discussed in Thread: CC2533, , Z-STACK
Tool/software:
On the CC2530 and CC2533, if the 802.15.4 PHY is used, but not the 802.15.4 MAC, is the Timer 2 (MAC Timer) needed? The user guide states
Timer 2 is mainly used to provide timing for 802.15.4 command-strobe-processor algorithms and for general timekeeping in the 802.15.4 MAC layer on CC253x devices,
Does this mean that it's needed when using the Program Execution mode with the CSP or does it apply to immediate command strobe execution as well (writing a single command to RFST).
However, in the CC2530B version of hal_sleep in Z-Stack 3.02, there is the following code.
/* power on the MAC; blocks until completion */ MAC_PwrOnReq();
HAL_ENABLE_INTERRUPTS();
/* For CC2530, T2 interrupt won’t be generated when the current count is greater than * the comparator. The interrupt is only generated when the current count is equal to * the comparator. When the CC2530 is waking up from sleep, there is a small window * that the count may be grater than the comparator, therefore, missing the interrupt. * This workaround will call the T2 ISR when the current T2 count is greater than the * comparator. The problem only occurs when POWER_SAVING is turned on, i.e. the 32KHz * drives the chip in sleep and SYNC start is used. */ macMcuTimer2OverflowWorkaround();
Does this matter if not using the 802.15.4 MAC layer?