This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Everyone,
I have two custom made PCB with CC2543 on it. I tried to transmit from one to another but I was not successful, Can someone please provide me with the sample code for transmitting and receiving using CC2543.
Thanks in advance
Prashanth
Hello Prashanth,
Have you tried using SmartRF studio for communicating between your boards? This is a straight forward way to verify that the hardware is functional. Sample code for CC2543 is available on its product page under tools and software tab.
http://www.ti.com/product/CC2543/toolssoftware
Regards,
Hello SVS,
Thanks for the reply, I have only one CC debugger.
Is there any other way to try SmartRF with one CC debugger and connect two CC2543 boards ?
I modified the PER test code to operate in Master beacon mode (text marked in red is what i have changed in the code to operate in master mode) and flashed it to one board and connected the other to SmartRf in packet RX mode, but i did not receive any packets. freq used : 2402 Mhz , modulation used : GFSK 250kbps 160khz
// Wait for user to press S1 to enter menu.
/* while(halButtonPushed() != HAL_BUTTON_1) {
#if(POWER_SAVING)
halSleepEnterPowerMode(CPU_HALT);
#endif
}*/
#if(POWER_SAVING)
// Interrupt disable on P0.1 (Button1).
P0IEN &= ~BIT1;
// Disable CPU Interrupt for Port 0 (IEN1.P0IE = 1).
P0IE = 0;
#endif
// Query user for operating mode.
// mode = queryMode();
mode = MASTER ;
if(mode == MASTER) {
while(1) {
// Start transmitting beacon packet every 10 ms.
masterBeaconMode();
do {
// Start PER terst in transmit mode.
runCondition = masterTxMode();
} while(runCondition == ACK_COMMAND_RESTART);
}
}
Regards,
Prashanth
Hello,
Try to download the code you downloaded from web onto both devices as there is a difference between the pre-loaded code and the latest version on web.
Also note that there might be a small bug in the argument given for the halRfSetFrequency() function where the incorrect frequency will be set. We will fix this in the next version.
Hello,
According to the last post in this thread, the code for the CC2543(www.ti.com/.../toolssoftware needs to be updated as per the stated bug in the previous post. Please update the code and send me to projects@distronix.in
We have tried with the software files provided in the TI site but failed to get the desired output.
To YiKai Chen,
I don't have the development kit with me so a lot of lcd stuff is needed to be removed from the code segments given. Moreover when I removed the LCD functionalities and tried to implement the core BLE broadcast the debug window was stuck at the interrupt section. I have attached the screenshot of the debug process where I am stuck right now.
Kindly help me to get through it.
Hello Aninda,
Use the software developed for the Mini Bluetooth® Low Energy Broadcaster board instead: