This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TRF7970A: DESFire EV1 AES encryption on the MSP432P401R

Part Number: TRF7970A
Other Parts Discussed in Thread: DLP-7970ABP

I've been assigned a project using RFID for one of our product lines.  So, I started out with the MSP432P401R launchpad along with the DLP-7970ABP booster pack and the NFC/HF RFID Reader / Writer application(SLOA227A).  Everything works great and I've learned a great deal.  Now the scope of the project has changed and we now want to use the DESFire tags because of the high level of encryption.  So, I found the DESFire EV1 AES Authentication app., SALOA213 and quickly realized that I had to port the code so that I could use it on the MSP432.  Everything was going fine until I ran into the MFDESFire folder in the project and the AES_Encryption library.  I need to rebuild the AES_Encryption.lib library to run on the MSP432 and there's no source code.  Were can I find it??  I've looked all over and have been unable to locate it.  Could some someone please point me in the correct direction?