Other Parts Discussed in Thread: MSP430FR4133
Hi everyone.
Past several days, I experimented with TRF7970A chip because I am using it on our project.
I think that I progressed a little bit on TRF7970A. But, at some of points I am in stuck. I explained below;
Project parameters : 3v3 power, SPI with SS, 14443A and 106 Kbps
Flow;
1. Enable chip (EN=H);
1. Cast SOFT RESET and IDLE
2. Configure Chip Status Reg
3. Configure ISO Control reg.
4. Configure Regulator reg.
5. Configure Modulator reg (13.56 Mhz crystal)
6. Configure NFC target det. level reg to 0x00 (for errata)
thus far everythin is normal. Am I right?
And then, rf power on, cast REQA.
Observations;
1. On the TX path 13.56 MHz sinusoidal signal (observed with oscilloscope and Vpeak-to-peak 5,5-6V arround)
2. After REQA commands I am receiving an interrupt form TRF, and reading IRQ stat reg.
a. if there is no a tag (Type-A 14443) near the antenna, I see only TX started flag (0x80)
b. if there is a tag (Type-A 14443) near the antenna, I see only TX started and RX started flag. (0xC0). But there is no second interrupt for RX comletion. Why?
c. When tag is near the antenna, after the rx start (but no interrupt), i read FIFO status and there is '2' number. It may be true because ATQA response is 2 byte. Am I right?
d. In FIFO register, there are 0x04 and 0x00 bytes. Are these ATQA response bytes?
Best reagards....