Hi team,
Please see the TRF7962A datasheet Figure 7-2. Impedance Matching Circuit.
C4,C5, C7 and C8, C9, C10, C11 are sensitive for different cap brand?
Thank you!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Zoe,
The cap brand/manufacturer isn't important but tolerance can be. Worst tolerance used should be 10%, but we recommend 5% is generally good enough but if a system is intended to be maximum performance than 1% is even better for that. Some of our EVM's use some 10% components though and the performance is still fine with that, but we wouldn't approve on our end of the use of anything higher than that.