Other Parts Discussed in Thread: TRF7960A
I use TRF7962A as my RFID Reader and ST Company's LRI2K as my TAG.
The communication protocol is ISO 15693.
So I have to get the UID of E0 02 xx xx ... when I read the UID normally.
The inventory command used is as follows:
command[0] = 0x8f;
command[0] = 0x91;
command[0] = 0x3d;
command[0] = 0x00;
command[0] = 0x30;
command[0] = 0x26;
command[0] = 0x01;
command[0] = 0x00;
This command was sent, then IRQ Register was initialized and the FIFO Status Register was read.
And then I read FIFO by size 10.
The IRQ register and FIFO were reset as the last step.
But why can't I get E0 and 02 data?