Hi Sub 1 Ghz team,
A customer is designing two boards. One will be Rx only, and the other will be Tx only. The frequency range is 940 to 960 MHz.
I'm expecting the CC1120EM-868-915-RD is a good starting point for the Rx.
On the Rx only board, can you give any guidance on how they should modify the components on the RF path to get the best performance at this frequency range? Are there passive components on the PA and TRX_SW pins that can be left off the board since it is Rx only?
Thanks,
Darren