This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1312: 915 MHz and 868 MHz channel list about Asia (China, Japan, Korea)

Does the frequency of 915 MHz and 868 MHz can pass Asia Telecommunications regulations (China, Japan, Korea)?

Do I just setup the frequency range and tx power to meet the regulations?

  • I would recommend reading the highlights in the Chinese, Japanese and Korean regulations before starting. As a general idea I believe you are correct, that you can either operate in the 868 MHz band or the 915 MHz band and adjust the frequency/ output power to comply. But regulations are normally more than that, typically setting max/ min on times, spurious transmission limits that in the end se the fundamental power, CCA/ LBT etc.