Other Parts Discussed in Thread: SYSCONFIG
Hi Team,
I am building a demo for a customer, where we need to send a small data package of a few bytes at a frequency of 10 Hz.
Therefore I used two LP-CC1352P-1 boards and reconfigured the senor and collector examples. For the 915MHz band at 50ksps I was able to reduce the reporting interval to 100ms and it worked fine.
Changing to the 868MHz band (same throughput of 50ksps) the maximum reporting frequency I could achieve was 9 Hz. The senor is just not sending data faster. Is this a limitation of the PHY or do i have to do more configuration work in the software?
Best regards,
Andreas