Other Parts Discussed in Thread: SYSCONFIG
Hello,
I have a couple of structs that I would like to initialise in the location that is used an NVS driver.
Currently I have set this as:
typedef struct __attribute((packed)) {
uint8_t FirstByte;
uint8_t SecondByte;
} struct_type;
#define DEFAULT_VALUES { .FirstByte = 0x00, .SecondByte = 0x01 }
struct_type structname __attribute__((packed, section("flashBuf0"), location(0x20000))) = DEFAULT_VALUES;
In my Syscfg file I have:
NVS1.$name = "CONFIG_NVS_0";
NVS1.internalFlash.$name = "ti_drivers_nvs_NVSCC26XX0";
NVS1.internalFlash.regionBase = 0x20000;
The error I get is:
error #10099-D: program will not fit into available memory, or the section contains a call site that requires a trampoline that can't be generated for this section. run placement with alignment fails for section ".TI.bound:flashBuf0" size 0x2000, overlaps with ".common:structname ", size 0x0002 (page 0)
Please inform me how I can resolve this.
Thank you,
Greg