Other Parts Discussed in Thread: CC1350, CC1310
Hi, SWRA642 says that the DSSS overrides should modify register 0x505C, but for CC1352P, SmartRF Studio modifies register 0x5068. The value for DSSS=2 is the same, 0x0100, but for DSSS=4 the value is also different than the one given in SWRA642, 0x030C rather than 0x0303.
Should I use the values from SmartRF Studio or the values from SWRA642? I used the values from SmartRF studio and I can get a CC1350 to hear a CC1352P, but I think with a high packet error rate. Not sure if this is the reason.
Also, is there any effect to setting these overrides (say to 0x0100) when fecMode=0, that is, when LRM is not used at all?
Thanks, Sivan Toledo