This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: Clock loss issue on the chip.

Part Number: CC1310
Other Parts Discussed in Thread: CC1190

Dear Sir/Ma'am,

We have developed one custom daughter board using the CC1310 chip which acts as Master in our application and communicates with slave devices (which are also based on the same CC1310 chip) on the same network.
We observed that it continually gets reset while communicating with its slave devices, Also the pattern of this Master reset is random, sometimes it occurs once or twice in an hour or it occurs continuously in every minute. Actually there was no consistent pattern of this reset on which we can track. We observed this issue when we connected this Master to the terminal of the computer (Tera term) and it showed the "[Reset-Source]:RSTSRC_CLK_LOSS" attached to the image of the terminal debug.
Initially we thought this issue is related to the external crystal mounted on the board may be that dry soldered or damaged. But when we checked that it looked like the crystal was soldered perfectly there was no issue with the external crystal. Attached is the image of that SCH. 
After that we checked the source of this clock loss issue in the firmware. So it seems that in the "sys_cltr.h" library provided by TI there is one function "SysCtrlResetSourceGet"
which returns one number and on  bases of that TI had provided the means of that number so in our case it is giving us the number 4 which means the clock loss. Please see attached image of that.
We need urgent support on this issue, Please have a look and let us know. 
Regards,
Hrishikesh.
  • Hi Hrishikesh,

    I agree this seems like an issue from your crystal.

    You can try disabling the clock loss detection feature. However this may lead to other issues if you indeed have clock loss in your system. 

    Please see the Technical Reference Manual section 6.7.1.1 Clock Loss Detection.

    https://www.ti.com/lit/swcu117

    Cheers,

    Marie H

  • Clock loss is not a known issue on this part meaning that if you have an issue you should request a schematic and layout review to verify that it's not something obvious wrong on the board. (https://www.ti.com/tool/SIMPLELINK-SUB1GHZ-DESIGN-REVIEWSf). The part of the schematic that you attached looks ok but the CC1190 or other path of the schematic could potentially cause issues. 

    Could you post the CCFG file to show how you have set up the chip and also the exact 24 MHz xtal you are using? 

  • Thanks Marie H & TheGhostOf  for your feedback.

    We are checking the Technical Reference Manual section 6.7.1.1 Clock Loss Detection.

    Also we shared the required all the documents on the "connectivity-sub1ghz-hw-review@list.ti.com" for the review 

    We hope we could get something on this issue.

    Thanks,

    Hrishikesh.

  • Hi Hrishiikesh,

    We are reviewing your design, and will provide a feedback within the end of next week. In the meantime, as TheGhostOf suggest, could you upload the CCFG file? It will help with the debugging.

    Best regards,

    Haiatullah

  • Dear ,

    Thanks for your reply,

    Would please give us idea of CCFG files? Then I immediately provide the those for review.

     

    Regards,

    Hrishikesh.  

  • Dear ,

    Could you please give us idea about the CCFG files? Then I immediately provide you those for your review.

    Regards,

    Hrishikesh

  • Dear ,

    Please ignore earlier query.

    I have attached  2 CCFG files first one which we programmed into the device named as "ccfg".

    Second one is the extracted from the faulty device named as "ccfg fetched from device".

    Regards,

    Hrishikesh.

    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 
    00 00 00 00 00 00 00 00 00 00 80 01 10 00 88 FF 
    FD FF 58 00 3A FF BF F3 FF FF FF FF FF FF FF FF 
    FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF 
    FF FF FF FF FF FF FF FF C5 0B FE C5 FF FF FF FF 
    00 FF FF FF C5 00 C5 FF 00 00 00 FF 00 00 00 00 
    FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF 
    
    /******************************************************************************
    *  Filename:       ccfg.c
    *  Revised:        $Date: 2017-08-08 15:34:36 +0200 (ti, 08 aug 2017) $
    *  Revision:       $Revision: 17873 $
    *
    *  Description:    Customer Configuration for CC13x0 device family (HW rev 2).
    *
    *  Copyright (C) 2014 Texas Instruments Incorporated - http://www.ti.com/
    *
    *
    *  Redistribution and use in source and binary forms, with or without
    *  modification, are permitted provided that the following conditions
    *  are met:
    *
    *    Redistributions of source code must retain the above copyright
    *    notice, this list of conditions and the following disclaimer.
    *
    *    Redistributions in binary form must reproduce the above copyright
    *    notice, this list of conditions and the following disclaimer in the
    *    documentation and/or other materials provided with the distribution.
    *
    *    Neither the name of Texas Instruments Incorporated nor the names of
    *    its contributors may be used to endorse or promote products derived
    *    from this software without specific prior written permission.
    *
    *  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
    *  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
    *  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
    *  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
    *  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
    *  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
    *  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
    *  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
    *  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
    *  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
    *  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    *
    ******************************************************************************/
    
    #ifndef __CCFC_C__
    #define __CCFC_C__
    
    #include <stdint.h>
    #include "../inc/hw_types.h"
    #include "../inc/hw_ccfg.h"
    #include "../inc/hw_ccfg_simple_struct.h"
    
    //*****************************************************************************
    //
    // Introduction
    //
    // This file contains fields used by Boot ROM, startup code, and SW radio
    // stacks to configure chip behavior.
    //
    // Fields are documented in more details in hw_ccfg.h and CCFG.html in
    // DriverLib documentation (doc_overview.html -> CPU Domain Memory Map -> CCFG).
    //
    // PLEASE NOTE:
    // It is not recommended to do modifications inside the ccfg.c file.
    // This file is part of the CoreSDK release and future releases may have
    // important modifications and new fields added without notice.
    // The recommended method to modify the CCFG settings is to have a separate
    // <customer_ccfg>.c file that defines the specific CCFG values to be
    // overridden and then include the TI provided ccfg.c at the very end,
    // giving default values for non-overriden settings.
    //
    // Example:
    // #define SET_CCFG_BL_CONFIG_BOOTLOADER_ENABLE  0xC5 // Enable ROM boot loader
    // #define SET_CCFG_MODE_CONF_SCLK_LF_OPTION     0x3  // LF RCOSC
    // //---- Use default values for all others ----
    // #include "<project-path>/source/ti/devices/<device>/startup_files/ccfg.c"
    //
    //*****************************************************************************
    
    //*****************************************************************************
    //
    // Internal settings, forcing several bit-fields to be set to a specific value.
    //
    //*****************************************************************************
    
    //#####################################
    // Force VDDR high setting (Higher output power but also higher power consumption)
    //#####################################
    
    #ifndef CCFG_FORCE_VDDR_HH
    #define CCFG_FORCE_VDDR_HH 0x0 // Use default VDDR trim
    // #define CCFG_FORCE_VDDR_HH                           0x1        // Force VDDR voltage to the factory HH setting (FCFG1..VDDR_TRIM_HH)
    #endif
    
    //*****************************************************************************
    //
    // Set the values of the individual bit fields.
    //
    //*****************************************************************************
    
    //#####################################
    // Alternative DC/DC settings
    //#####################################
    
    #ifndef SET_CCFG_SIZE_AND_DIS_FLAGS_DIS_ALT_DCDC_SETTING
    #define SET_CCFG_SIZE_AND_DIS_FLAGS_DIS_ALT_DCDC_SETTING 0x0 // Alternative DC/DC setting enabled
    // #define SET_CCFG_SIZE_AND_DIS_FLAGS_DIS_ALT_DCDC_SETTING 0x1    // Alternative DC/DC setting disabled
    #endif
    
    #if (CCFG_FORCE_VDDR_HH)
    #define SET_CCFG_MODE_CONF_1_ALT_DCDC_VMIN 0xC // Special VMIN level (2.5V) when forced VDDR HH voltage
    #else
    #ifndef SET_CCFG_MODE_CONF_1_ALT_DCDC_VMIN
    #define SET_CCFG_MODE_CONF_1_ALT_DCDC_VMIN 0x8 // 2.25V
    #endif
    #endif
    
    #ifndef SET_CCFG_MODE_CONF_1_ALT_DCDC_DITHER_EN
    // #define SET_CCFG_MODE_CONF_1_ALT_DCDC_DITHER_EN          0x0    // Disable
    #define SET_CCFG_MODE_CONF_1_ALT_DCDC_DITHER_EN 0x1 // Enable
    #endif
    
    #ifndef SET_CCFG_MODE_CONF_1_ALT_DCDC_IPEAK
    #define SET_CCFG_MODE_CONF_1_ALT_DCDC_IPEAK 0x0 // 31mA
    #endif
    
    //#####################################
    // XOSC override settings
    //#####################################
    
    #ifndef SET_CCFG_SIZE_AND_DIS_FLAGS_DIS_XOSC_OVR
    // #define SET_CCFG_SIZE_AND_DIS_FLAGS_DIS_XOSC_OVR     0x0        // Enable override
    #define SET_CCFG_SIZE_AND_DIS_FLAGS_DIS_XOSC_OVR 0x1 // Disable override
    #endif
    
    #ifndef SET_CCFG_MODE_CONF_1_DELTA_IBIAS_INIT
    #define SET_CCFG_MODE_CONF_1_DELTA_IBIAS_INIT 0x0 // Delta = 0
    #endif
    
    #ifndef SET_CCFG_MODE_CONF_1_DELTA_IBIAS_OFFSET
    #define SET_CCFG_MODE_CONF_1_DELTA_IBIAS_OFFSET 0x0 // Delta = 0
    #endif
    
    #ifndef SET_CCFG_MODE_CONF_1_XOSC_MAX_START
    #define SET_CCFG_MODE_CONF_1_XOSC_MAX_START 0x10 // 1600us
    #endif
    
    //#####################################
    // Power settings
    //#####################################
    
    #ifndef SET_CCFG_MODE_CONF_VDDR_TRIM_SLEEP_DELTA
    #define SET_CCFG_MODE_CONF_VDDR_TRIM_SLEEP_DELTA 0xF // Signed delta value +1 to apply to the VDDR_TRIM_SLEEP target (0xF=-1=default=no compensation)
    #endif
    
    #ifndef SET_CCFG_MODE_CONF_DCDC_RECHARGE
    #define SET_CCFG_MODE_CONF_DCDC_RECHARGE 0x0 // Use the DC/DC during recharge in powerdown
    // #define SET_CCFG_MODE_CONF_DCDC_RECHARGE             0x1        // Do not use the DC/DC during recharge in powerdown
    #endif
    
    #ifndef SET_CCFG_MODE_CONF_DCDC_ACTIVE
    #define SET_CCFG_MODE_CONF_DCDC_ACTIVE 0x0 // Use the DC/DC during active mode
    // #define SET_CCFG_MODE_CONF_DCDC_ACTIVE               0x1        // Do not use the DC/DC during active mode
    #endif
    
    #if (CCFG_FORCE_VDDR_HH)
    #define SET_CCFG_MODE_CONF_VDDS_BOD_LEVEL 0x1 // Special setting to enable forced VDDR HH voltage
    #else
    #ifndef SET_CCFG_MODE_CONF_VDDS_BOD_LEVEL
    // #define SET_CCFG_MODE_CONF_VDDS_BOD_LEVEL            0x0        // VDDS BOD level is 2.0V
    #define SET_CCFG_MODE_CONF_VDDS_BOD_LEVEL 0x1 // VDDS BOD level is 1.8V (or 1.65V for external regulator mode)
    #endif
    #endif
    
    #ifndef SET_CCFG_MODE_CONF_VDDR_CAP
    #define SET_CCFG_MODE_CONF_VDDR_CAP 0x3A // Unsigned 8-bit integer representing the min. decoupling capacitance on VDDR in units of 100nF
    #endif
    
    #ifndef SET_CCFG_MODE_CONF_VDDR_TRIM_SLEEP_TC
    #define SET_CCFG_MODE_CONF_VDDR_TRIM_SLEEP_TC 0x1 // Temperature compensation on VDDR sleep trim disabled (default)
    // #define SET_CCFG_MODE_CONF_VDDR_TRIM_SLEEP_TC        0x0        // Temperature compensation on VDDR sleep trim enabled
    #endif
    
    //#####################################
    // Clock settings
    //#####################################
    
    #ifndef SET_CCFG_MODE_CONF_SCLK_LF_OPTION
    // #define SET_CCFG_MODE_CONF_SCLK_LF_OPTION            0x0        // LF clock derived from High Frequency XOSC
    // #define SET_CCFG_MODE_CONF_SCLK_LF_OPTION            0x1        // External LF clock
    #define SET_CCFG_MODE_CONF_SCLK_LF_OPTION 0x2 // LF XOSC
    // #define SET_CCFG_MODE_CONF_SCLK_LF_OPTION            0x3        // LF RCOSC
    #endif
    
    #ifndef SET_CCFG_MODE_CONF_XOSC_CAP_MOD
    // #define SET_CCFG_MODE_CONF_XOSC_CAP_MOD              0x0        // Apply cap-array delta
    #define SET_CCFG_MODE_CONF_XOSC_CAP_MOD 0x1 // Don't apply cap-array delta
    #endif
    
    #ifndef SET_CCFG_MODE_CONF_XOSC_CAPARRAY_DELTA
    #define SET_CCFG_MODE_CONF_XOSC_CAPARRAY_DELTA 0xFF // Signed 8-bit value, directly modifying trimmed XOSC cap-array value
    #endif
    
    #ifndef SET_CCFG_EXT_LF_CLK_DIO
    #define SET_CCFG_EXT_LF_CLK_DIO 0x01 // DIO number if using external LF clock
    #endif
    
    #ifndef SET_CCFG_EXT_LF_CLK_RTC_INCREMENT
    #define SET_CCFG_EXT_LF_CLK_RTC_INCREMENT 0x800000 // RTC increment representing the external LF clock frequency
    #endif
    
    //#####################################
    // Special HF clock source setting
    //#####################################
    #ifndef SET_CCFG_MODE_CONF_XOSC_FREQ
    // #define SET_CCFG_MODE_CONF_XOSC_FREQ                 0x1        // Use HPOSC as HF source (Unavailable on CC13xx chips)
    // #define SET_CCFG_MODE_CONF_XOSC_FREQ                 0x2        // HF source is a 48 MHz xtal
    #define SET_CCFG_MODE_CONF_XOSC_FREQ 0x3 // HF source is a 24 MHz xtal (default)
    #endif
    
    //#####################################
    // Bootloader settings
    //#####################################
    
    #ifndef SET_CCFG_BL_CONFIG_BOOTLOADER_ENABLE
    //#define SET_CCFG_BL_CONFIG_BOOTLOADER_ENABLE            0x00       // Disable ROM boot loader
    #define SET_CCFG_BL_CONFIG_BOOTLOADER_ENABLE 0xC5 // Enable ROM boot loader
    #endif
    
    #ifndef SET_CCFG_BL_CONFIG_BL_LEVEL
    #define SET_CCFG_BL_CONFIG_BL_LEVEL 0x0 // Active low to open boot loader backdoor
    //#define SET_CCFG_BL_CONFIG_BL_LEVEL                     0x1        // Active high to open boot loader backdoor
    #endif
    
    #ifndef SET_CCFG_BL_CONFIG_BL_PIN_NUMBER
    #define SET_CCFG_BL_CONFIG_BL_PIN_NUMBER 0x0B // DIO number for boot loader backdoor
    #endif
    
    #ifndef SET_CCFG_BL_CONFIG_BL_ENABLE
    #define SET_CCFG_BL_CONFIG_BL_ENABLE 0xC5 // Enabled boot loader backdoor
    //#define SET_CCFG_BL_CONFIG_BL_ENABLE                    0xFF       // Disabled boot loader backdoor
    #endif
    
    //#####################################
    // Debug access settings
    //#####################################
    
    #ifndef SET_CCFG_CCFG_TI_OPTIONS_TI_FA_ENABLE
    #define SET_CCFG_CCFG_TI_OPTIONS_TI_FA_ENABLE 0x00 // Disable unlocking of TI FA option
    // #define SET_CCFG_CCFG_TI_OPTIONS_TI_FA_ENABLE        0xC5       // Enable unlocking of TI FA option with the unlock code
    #endif
    
    #ifndef SET_CCFG_CCFG_TAP_DAP_0_CPU_DAP_ENABLE
    // #define SET_CCFG_CCFG_TAP_DAP_0_CPU_DAP_ENABLE       0x00       // Access disabled
    #define SET_CCFG_CCFG_TAP_DAP_0_CPU_DAP_ENABLE 0xC5 // Access enabled if also enabled in FCFG
    #endif
    
    #ifndef SET_CCFG_CCFG_TAP_DAP_0_PRCM_TAP_ENABLE
    #define SET_CCFG_CCFG_TAP_DAP_0_PRCM_TAP_ENABLE 0x00 // Access disabled
    // #define SET_CCFG_CCFG_TAP_DAP_0_PRCM_TAP_ENABLE      0xC5       // Access enabled if also enabled in FCFG
    #endif
    
    #ifndef SET_CCFG_CCFG_TAP_DAP_0_TEST_TAP_ENABLE
    // #define SET_CCFG_CCFG_TAP_DAP_0_TEST_TAP_ENABLE      0x00       // Access disabled
    #define SET_CCFG_CCFG_TAP_DAP_0_TEST_TAP_ENABLE 0xC5 // Access enabled if also enabled in FCFG
    #endif
    
    #ifndef SET_CCFG_CCFG_TAP_DAP_1_PBIST2_TAP_ENABLE
    #define SET_CCFG_CCFG_TAP_DAP_1_PBIST2_TAP_ENABLE 0x00 // Access disabled
    // #define SET_CCFG_CCFG_TAP_DAP_1_PBIST2_TAP_ENABLE    0xC5       // Access enabled if also enabled in FCFG
    #endif
    
    #ifndef SET_CCFG_CCFG_TAP_DAP_1_PBIST1_TAP_ENABLE
    #define SET_CCFG_CCFG_TAP_DAP_1_PBIST1_TAP_ENABLE 0x00 // Access disabled
    // #define SET_CCFG_CCFG_TAP_DAP_1_PBIST1_TAP_ENABLE    0xC5       // Access enabled if also enabled in FCFG
    #endif
    
    #ifndef SET_CCFG_CCFG_TAP_DAP_1_WUC_TAP_ENABLE
    #define SET_CCFG_CCFG_TAP_DAP_1_WUC_TAP_ENABLE 0x00 // Access disabled
    // #define SET_CCFG_CCFG_TAP_DAP_1_WUC_TAP_ENABLE       0xC5       // Access enabled if also enabled in FCFG
    #endif
    
    //#####################################
    // Alternative IEEE 802.15.4 MAC address
    //#####################################
    #ifndef SET_CCFG_IEEE_MAC_0
    #define SET_CCFG_IEEE_MAC_0 0xFFFFFFFF // Bits [31:0]
    #endif
    
    #ifndef SET_CCFG_IEEE_MAC_1
    #define SET_CCFG_IEEE_MAC_1 0xFFFFFFFF // Bits [63:32]
    #endif
    
    //#####################################
    // Alternative BLE address
    //#####################################
    #ifndef SET_CCFG_IEEE_BLE_0
    #define SET_CCFG_IEEE_BLE_0 0xFFFFFFFF // Bits [31:0]
    #endif
    
    #ifndef SET_CCFG_IEEE_BLE_1
    #define SET_CCFG_IEEE_BLE_1 0xFFFFFFFF // Bits [63:32]
    #endif
    
    //#####################################
    // Flash erase settings
    //#####################################
    
    #ifndef SET_CCFG_ERASE_CONF_CHIP_ERASE_DIS_N
    // #define SET_CCFG_ERASE_CONF_CHIP_ERASE_DIS_N         0x0        // Any chip erase request detected during boot will be ignored
    #define SET_CCFG_ERASE_CONF_CHIP_ERASE_DIS_N 0x1 // Any chip erase request detected during boot will be performed by the boot FW
    #endif
    
    #ifndef SET_CCFG_ERASE_CONF_BANK_ERASE_DIS_N
    // #define SET_CCFG_ERASE_CONF_BANK_ERASE_DIS_N         0x0        // Disable the boot loader bank erase function
    #define SET_CCFG_ERASE_CONF_BANK_ERASE_DIS_N 0x1 // Enable the boot loader bank erase function
    #endif
    
    //#####################################
    // Flash image valid
    //#####################################
    #ifndef SET_CCFG_IMAGE_VALID_CONF_IMAGE_VALID
    #define SET_CCFG_IMAGE_VALID_CONF_IMAGE_VALID 0x00000000 // Flash image is valid
    // #define SET_CCFG_IMAGE_VALID_CONF_IMAGE_VALID        <non-zero> // Flash image is invalid. ROM boot loader is called.
    #endif
    
    //#####################################
    // Flash sector write protection
    //#####################################
    #ifndef SET_CCFG_CCFG_PROT_31_0
    #define SET_CCFG_CCFG_PROT_31_0 0xFFFFFFFF
    #endif
    
    #ifndef SET_CCFG_CCFG_PROT_63_32
    #define SET_CCFG_CCFG_PROT_63_32 0xFFFFFFFF
    #endif
    
    #ifndef SET_CCFG_CCFG_PROT_95_64
    #define SET_CCFG_CCFG_PROT_95_64 0xFFFFFFFF
    #endif
    
    #ifndef SET_CCFG_CCFG_PROT_127_96
    #define SET_CCFG_CCFG_PROT_127_96 0xFFFFFFFF
    #endif
    
    //#####################################
    // Select between cache or GPRAM
    //#####################################
    #ifndef SET_CCFG_SIZE_AND_DIS_FLAGS_DIS_GPRAM
    // #define SET_CCFG_SIZE_AND_DIS_FLAGS_DIS_GPRAM        0x0        // Cache is disabled and GPRAM is available at 0x11000000-0x11001FFF
    #define SET_CCFG_SIZE_AND_DIS_FLAGS_DIS_GPRAM 0x1 // Cache is enabled and GPRAM is disabled (unavailable)
    #endif
    
    //#####################################
    // Select TCXO
    //#####################################
    #ifndef SET_CCFG_SIZE_AND_DIS_FLAGS_DIS_TCXO
    #define SET_CCFG_SIZE_AND_DIS_FLAGS_DIS_TCXO 0x1 // Disable TCXO
    // #define SET_CCFG_SIZE_AND_DIS_FLAGS_DIS_TCXO         0x0    // Enable TXCO
    #endif
    
    //*****************************************************************************
    //
    // CCFG values that should not be modified.
    //
    //*****************************************************************************
    #define SET_CCFG_SIZE_AND_DIS_FLAGS_SIZE_OF_CCFG 0x0058
    #define SET_CCFG_SIZE_AND_DIS_FLAGS_DISABLE_FLAGS (CCFG_SIZE_AND_DIS_FLAGS_DISABLE_FLAGS_M >> CCFG_SIZE_AND_DIS_FLAGS_DISABLE_FLAGS_S)
    
    #if (CCFG_FORCE_VDDR_HH)
    #define SET_CCFG_MODE_CONF_VDDR_EXT_LOAD 0x0 // Special setting to enable forced VDDR HH voltage
    #else
    #define SET_CCFG_MODE_CONF_VDDR_EXT_LOAD 0x1
    #endif
    
    #define SET_CCFG_MODE_CONF_RTC_COMP 0x1
    #define SET_CCFG_MODE_CONF_HF_COMP 0x1
    
    #define SET_CCFG_VOLT_LOAD_0_VDDR_EXT_TP45 0xFF
    #define SET_CCFG_VOLT_LOAD_0_VDDR_EXT_TP25 0xFF
    #define SET_CCFG_VOLT_LOAD_0_VDDR_EXT_TP5 0xFF
    #define SET_CCFG_VOLT_LOAD_0_VDDR_EXT_TM15 0xFF
    
    #define SET_CCFG_VOLT_LOAD_1_VDDR_EXT_TP125 0xFF
    #define SET_CCFG_VOLT_LOAD_1_VDDR_EXT_TP105 0xFF
    #define SET_CCFG_VOLT_LOAD_1_VDDR_EXT_TP85 0xFF
    #define SET_CCFG_VOLT_LOAD_1_VDDR_EXT_TP65 0xFF
    
    #define SET_CCFG_RTC_OFFSET_RTC_COMP_P0 0xFFFF
    #define SET_CCFG_RTC_OFFSET_RTC_COMP_P1 0xFF
    #define SET_CCFG_RTC_OFFSET_RTC_COMP_P2 0xFF
    
    #define SET_CCFG_FREQ_OFFSET_HF_COMP_P0 0xFFFF
    #define SET_CCFG_FREQ_OFFSET_HF_COMP_P1 0xFF
    #define SET_CCFG_FREQ_OFFSET_HF_COMP_P2 0xFF
    
    //*****************************************************************************
    //
    // Concatenate bit fields to words.
    // DO NOT EDIT!
    //
    //*****************************************************************************
    #define DEFAULT_CCFG_EXT_LF_CLK (                                                                 \
    ((((uint32_t)(SET_CCFG_EXT_LF_CLK_DIO)) << CCFG_EXT_LF_CLK_DIO_S) | ~CCFG_EXT_LF_CLK_DIO_M) & \
    	((((uint32_t)(SET_CCFG_EXT_LF_CLK_RTC_INCREMENT)) << CCFG_EXT_LF_CLK_RTC_INCREMENT_S) | ~CCFG_EXT_LF_CLK_RTC_INCREMENT_M))
    
    #define DEFAULT_CCFG_MODE_CONF_1 (                                                                                                                \
    ((((uint32_t)(SET_CCFG_MODE_CONF_1_ALT_DCDC_VMIN)) << CCFG_MODE_CONF_1_ALT_DCDC_VMIN_S) | ~CCFG_MODE_CONF_1_ALT_DCDC_VMIN_M) &                \
    	((((uint32_t)(SET_CCFG_MODE_CONF_1_ALT_DCDC_DITHER_EN)) << CCFG_MODE_CONF_1_ALT_DCDC_DITHER_EN_S) | ~CCFG_MODE_CONF_1_ALT_DCDC_DITHER_EN_M) & \
            ((((uint32_t)(SET_CCFG_MODE_CONF_1_ALT_DCDC_IPEAK)) << CCFG_MODE_CONF_1_ALT_DCDC_IPEAK_S) | ~CCFG_MODE_CONF_1_ALT_DCDC_IPEAK_M) &             \
                ((((uint32_t)(SET_CCFG_MODE_CONF_1_DELTA_IBIAS_INIT)) << CCFG_MODE_CONF_1_DELTA_IBIAS_INIT_S) | ~CCFG_MODE_CONF_1_DELTA_IBIAS_INIT_M) &       \
                    ((((uint32_t)(SET_CCFG_MODE_CONF_1_DELTA_IBIAS_OFFSET)) << CCFG_MODE_CONF_1_DELTA_IBIAS_OFFSET_S) | ~CCFG_MODE_CONF_1_DELTA_IBIAS_OFFSET_M) & \
                        ((((uint32_t)(SET_CCFG_MODE_CONF_1_XOSC_MAX_START)) << CCFG_MODE_CONF_1_XOSC_MAX_START_S) | ~CCFG_MODE_CONF_1_XOSC_MAX_START_M))
    
    #define DEFAULT_CCFG_SIZE_AND_DIS_FLAGS (                                                                                                                                    \
    ((((uint32_t)(SET_CCFG_SIZE_AND_DIS_FLAGS_SIZE_OF_CCFG)) << CCFG_SIZE_AND_DIS_FLAGS_SIZE_OF_CCFG_S) | ~CCFG_SIZE_AND_DIS_FLAGS_SIZE_OF_CCFG_M) &                         \
    	((((uint32_t)(SET_CCFG_SIZE_AND_DIS_FLAGS_DISABLE_FLAGS)) << CCFG_SIZE_AND_DIS_FLAGS_DISABLE_FLAGS_S) | ~CCFG_SIZE_AND_DIS_FLAGS_DISABLE_FLAGS_M) &                      \
            ((((uint32_t)(SET_CCFG_SIZE_AND_DIS_FLAGS_DIS_TCXO)) << CCFG_SIZE_AND_DIS_FLAGS_DIS_TCXO_S) | ~CCFG_SIZE_AND_DIS_FLAGS_DIS_TCXO_M) &                                     \
                ((((uint32_t)(SET_CCFG_SIZE_AND_DIS_FLAGS_DIS_GPRAM)) << CCFG_SIZE_AND_DIS_FLAGS_DIS_GPRAM_S) | ~CCFG_SIZE_AND_DIS_FLAGS_DIS_GPRAM_M) &                                  \
                    ((((uint32_t)(SET_CCFG_SIZE_AND_DIS_FLAGS_DIS_ALT_DCDC_SETTING)) << CCFG_SIZE_AND_DIS_FLAGS_DIS_ALT_DCDC_SETTING_S) | ~CCFG_SIZE_AND_DIS_FLAGS_DIS_ALT_DCDC_SETTING_M) & \
                        ((((uint32_t)(SET_CCFG_SIZE_AND_DIS_FLAGS_DIS_XOSC_OVR)) << CCFG_SIZE_AND_DIS_FLAGS_DIS_XOSC_OVR_S) | ~CCFG_SIZE_AND_DIS_FLAGS_DIS_XOSC_OVR_M))
    
    #define DEFAULT_CCFG_MODE_CONF (                                                                                                                     \
    ((((uint32_t)(SET_CCFG_MODE_CONF_VDDR_TRIM_SLEEP_DELTA)) << CCFG_MODE_CONF_VDDR_TRIM_SLEEP_DELTA_S) | ~CCFG_MODE_CONF_VDDR_TRIM_SLEEP_DELTA_M) & \
    	((((uint32_t)(SET_CCFG_MODE_CONF_DCDC_RECHARGE)) << CCFG_MODE_CONF_DCDC_RECHARGE_S) | ~CCFG_MODE_CONF_DCDC_RECHARGE_M) &                         \
            ((((uint32_t)(SET_CCFG_MODE_CONF_DCDC_ACTIVE)) << CCFG_MODE_CONF_DCDC_ACTIVE_S) | ~CCFG_MODE_CONF_DCDC_ACTIVE_M) &                               \
                ((((uint32_t)(SET_CCFG_MODE_CONF_VDDR_EXT_LOAD)) << CCFG_MODE_CONF_VDDR_EXT_LOAD_S) | ~CCFG_MODE_CONF_VDDR_EXT_LOAD_M) &                         \
                    ((((uint32_t)(SET_CCFG_MODE_CONF_VDDS_BOD_LEVEL)) << CCFG_MODE_CONF_VDDS_BOD_LEVEL_S) | ~CCFG_MODE_CONF_VDDS_BOD_LEVEL_M) &                      \
                        ((((uint32_t)(SET_CCFG_MODE_CONF_SCLK_LF_OPTION)) << CCFG_MODE_CONF_SCLK_LF_OPTION_S) | ~CCFG_MODE_CONF_SCLK_LF_OPTION_M) &                      \
                            ((((uint32_t)(SET_CCFG_MODE_CONF_VDDR_TRIM_SLEEP_TC)) << CCFG_MODE_CONF_VDDR_TRIM_SLEEP_TC_S) | ~CCFG_MODE_CONF_VDDR_TRIM_SLEEP_TC_M) &          \
                                ((((uint32_t)(SET_CCFG_MODE_CONF_RTC_COMP)) << CCFG_MODE_CONF_RTC_COMP_S) | ~CCFG_MODE_CONF_RTC_COMP_M) &                                        \
                                    ((((uint32_t)(SET_CCFG_MODE_CONF_XOSC_FREQ)) << CCFG_MODE_CONF_XOSC_FREQ_S) | ~CCFG_MODE_CONF_XOSC_FREQ_M) &                                     \
                                        ((((uint32_t)(SET_CCFG_MODE_CONF_XOSC_CAP_MOD)) << CCFG_MODE_CONF_XOSC_CAP_MOD_S) | ~CCFG_MODE_CONF_XOSC_CAP_MOD_M) &                            \
                                            ((((uint32_t)(SET_CCFG_MODE_CONF_HF_COMP)) << CCFG_MODE_CONF_HF_COMP_S) | ~CCFG_MODE_CONF_HF_COMP_M) &                                           \
                                                ((((uint32_t)(SET_CCFG_MODE_CONF_XOSC_CAPARRAY_DELTA)) << CCFG_MODE_CONF_XOSC_CAPARRAY_DELTA_S) | ~CCFG_MODE_CONF_XOSC_CAPARRAY_DELTA_M) &       \
                                                    ((((uint32_t)(SET_CCFG_MODE_CONF_VDDR_CAP)) << CCFG_MODE_CONF_VDDR_CAP_S) | ~CCFG_MODE_CONF_VDDR_CAP_M))
    
    #define DEFAULT_CCFG_VOLT_LOAD_0 (                                                                                                 \
    ((((uint32_t)(SET_CCFG_VOLT_LOAD_0_VDDR_EXT_TP45)) << CCFG_VOLT_LOAD_0_VDDR_EXT_TP45_S) | ~CCFG_VOLT_LOAD_0_VDDR_EXT_TP45_M) & \
    	((((uint32_t)(SET_CCFG_VOLT_LOAD_0_VDDR_EXT_TP25)) << CCFG_VOLT_LOAD_0_VDDR_EXT_TP25_S) | ~CCFG_VOLT_LOAD_0_VDDR_EXT_TP25_M) & \
            ((((uint32_t)(SET_CCFG_VOLT_LOAD_0_VDDR_EXT_TP5)) << CCFG_VOLT_LOAD_0_VDDR_EXT_TP5_S) | ~CCFG_VOLT_LOAD_0_VDDR_EXT_TP5_M) &    \
                ((((uint32_t)(SET_CCFG_VOLT_LOAD_0_VDDR_EXT_TM15)) << CCFG_VOLT_LOAD_0_VDDR_EXT_TM15_S) | ~CCFG_VOLT_LOAD_0_VDDR_EXT_TM15_M))
    
    #define DEFAULT_CCFG_VOLT_LOAD_1 (                                                                                                    \
    ((((uint32_t)(SET_CCFG_VOLT_LOAD_1_VDDR_EXT_TP125)) << CCFG_VOLT_LOAD_1_VDDR_EXT_TP125_S) | ~CCFG_VOLT_LOAD_1_VDDR_EXT_TP125_M) & \
    	((((uint32_t)(SET_CCFG_VOLT_LOAD_1_VDDR_EXT_TP105)) << CCFG_VOLT_LOAD_1_VDDR_EXT_TP105_S) | ~CCFG_VOLT_LOAD_1_VDDR_EXT_TP105_M) & \
            ((((uint32_t)(SET_CCFG_VOLT_LOAD_1_VDDR_EXT_TP85)) << CCFG_VOLT_LOAD_1_VDDR_EXT_TP85_S) | ~CCFG_VOLT_LOAD_1_VDDR_EXT_TP85_M) &    \
                ((((uint32_t)(SET_CCFG_VOLT_LOAD_1_VDDR_EXT_TP65)) << CCFG_VOLT_LOAD_1_VDDR_EXT_TP65_S) | ~CCFG_VOLT_LOAD_1_VDDR_EXT_TP65_M))
    
    #define DEFAULT_CCFG_RTC_OFFSET (                                                                                         \
    ((((uint32_t)(SET_CCFG_RTC_OFFSET_RTC_COMP_P0)) << CCFG_RTC_OFFSET_RTC_COMP_P0_S) | ~CCFG_RTC_OFFSET_RTC_COMP_P0_M) & \
    	((((uint32_t)(SET_CCFG_RTC_OFFSET_RTC_COMP_P1)) << CCFG_RTC_OFFSET_RTC_COMP_P1_S) | ~CCFG_RTC_OFFSET_RTC_COMP_P1_M) & \
            ((((uint32_t)(SET_CCFG_RTC_OFFSET_RTC_COMP_P2)) << CCFG_RTC_OFFSET_RTC_COMP_P2_S) | ~CCFG_RTC_OFFSET_RTC_COMP_P2_M))
    
    #define DEFAULT_CCFG_FREQ_OFFSET (                                                                                        \
    ((((uint32_t)(SET_CCFG_FREQ_OFFSET_HF_COMP_P0)) << CCFG_FREQ_OFFSET_HF_COMP_P0_S) | ~CCFG_FREQ_OFFSET_HF_COMP_P0_M) & \
    	((((uint32_t)(SET_CCFG_FREQ_OFFSET_HF_COMP_P1)) << CCFG_FREQ_OFFSET_HF_COMP_P1_S) | ~CCFG_FREQ_OFFSET_HF_COMP_P1_M) & \
            ((((uint32_t)(SET_CCFG_FREQ_OFFSET_HF_COMP_P2)) << CCFG_FREQ_OFFSET_HF_COMP_P2_S) | ~CCFG_FREQ_OFFSET_HF_COMP_P2_M))
    
    #define DEFAULT_CCFG_IEEE_MAC_0 SET_CCFG_IEEE_MAC_0
    #define DEFAULT_CCFG_IEEE_MAC_1 SET_CCFG_IEEE_MAC_1
    #define DEFAULT_CCFG_IEEE_BLE_0 SET_CCFG_IEEE_BLE_0
    #define DEFAULT_CCFG_IEEE_BLE_1 SET_CCFG_IEEE_BLE_1
    
    #define DEFAULT_CCFG_BL_CONFIG (                                                                                                         \
    ((((uint32_t)(SET_CCFG_BL_CONFIG_BOOTLOADER_ENABLE)) << CCFG_BL_CONFIG_BOOTLOADER_ENABLE_S) | ~CCFG_BL_CONFIG_BOOTLOADER_ENABLE_M) & \
    	((((uint32_t)(SET_CCFG_BL_CONFIG_BL_LEVEL)) << CCFG_BL_CONFIG_BL_LEVEL_S) | ~CCFG_BL_CONFIG_BL_LEVEL_M) &                            \
            ((((uint32_t)(SET_CCFG_BL_CONFIG_BL_PIN_NUMBER)) << CCFG_BL_CONFIG_BL_PIN_NUMBER_S) | ~CCFG_BL_CONFIG_BL_PIN_NUMBER_M) &             \
                ((((uint32_t)(SET_CCFG_BL_CONFIG_BL_ENABLE)) << CCFG_BL_CONFIG_BL_ENABLE_S) | ~CCFG_BL_CONFIG_BL_ENABLE_M))
    
    #define DEFAULT_CCFG_ERASE_CONF (                                                                                                        \
    ((((uint32_t)(SET_CCFG_ERASE_CONF_CHIP_ERASE_DIS_N)) << CCFG_ERASE_CONF_CHIP_ERASE_DIS_N_S) | ~CCFG_ERASE_CONF_CHIP_ERASE_DIS_N_M) & \
    	((((uint32_t)(SET_CCFG_ERASE_CONF_BANK_ERASE_DIS_N)) << CCFG_ERASE_CONF_BANK_ERASE_DIS_N_S) | ~CCFG_ERASE_CONF_BANK_ERASE_DIS_N_M))
    
    #define DEFAULT_CCFG_CCFG_TI_OPTIONS ( \
    ((((uint32_t)(SET_CCFG_CCFG_TI_OPTIONS_TI_FA_ENABLE)) << CCFG_CCFG_TI_OPTIONS_TI_FA_ENABLE_S) | ~CCFG_CCFG_TI_OPTIONS_TI_FA_ENABLE_M))
    
    #define DEFAULT_CCFG_CCFG_TAP_DAP_0 (                                                                                                             \
    ((((uint32_t)(SET_CCFG_CCFG_TAP_DAP_0_CPU_DAP_ENABLE)) << CCFG_CCFG_TAP_DAP_0_CPU_DAP_ENABLE_S) | ~CCFG_CCFG_TAP_DAP_0_CPU_DAP_ENABLE_M) &    \
    	((((uint32_t)(SET_CCFG_CCFG_TAP_DAP_0_PRCM_TAP_ENABLE)) << CCFG_CCFG_TAP_DAP_0_PRCM_TAP_ENABLE_S) | ~CCFG_CCFG_TAP_DAP_0_PRCM_TAP_ENABLE_M) & \
            ((((uint32_t)(SET_CCFG_CCFG_TAP_DAP_0_TEST_TAP_ENABLE)) << CCFG_CCFG_TAP_DAP_0_TEST_TAP_ENABLE_S) | ~CCFG_CCFG_TAP_DAP_0_TEST_TAP_ENABLE_M))
    
    #define DEFAULT_CCFG_CCFG_TAP_DAP_1 (                                                                                                                   \
    ((((uint32_t)(SET_CCFG_CCFG_TAP_DAP_1_PBIST2_TAP_ENABLE)) << CCFG_CCFG_TAP_DAP_1_PBIST2_TAP_ENABLE_S) | ~CCFG_CCFG_TAP_DAP_1_PBIST2_TAP_ENABLE_M) & \
    	((((uint32_t)(SET_CCFG_CCFG_TAP_DAP_1_PBIST1_TAP_ENABLE)) << CCFG_CCFG_TAP_DAP_1_PBIST1_TAP_ENABLE_S) | ~CCFG_CCFG_TAP_DAP_1_PBIST1_TAP_ENABLE_M) & \
            ((((uint32_t)(SET_CCFG_CCFG_TAP_DAP_1_WUC_TAP_ENABLE)) << CCFG_CCFG_TAP_DAP_1_WUC_TAP_ENABLE_S) | ~CCFG_CCFG_TAP_DAP_1_WUC_TAP_ENABLE_M))
    
    #define DEFAULT_CCFG_IMAGE_VALID_CONF SET_CCFG_IMAGE_VALID_CONF_IMAGE_VALID
    
    #define DEFAULT_CCFG_CCFG_PROT_31_0 SET_CCFG_CCFG_PROT_31_0
    #define DEFAULT_CCFG_CCFG_PROT_63_32 SET_CCFG_CCFG_PROT_63_32
    #define DEFAULT_CCFG_CCFG_PROT_95_64 SET_CCFG_CCFG_PROT_95_64
    #define DEFAULT_CCFG_CCFG_PROT_127_96 SET_CCFG_CCFG_PROT_127_96
    
    //*****************************************************************************
    //
    // Customer Configuration Area in Lock Page
    //
    //*****************************************************************************
    #if defined(__IAR_SYSTEMS_ICC__)
    __root const ccfg_t __ccfg @ ".ccfg" =
    #elif defined(__TI_COMPILER_VERSION__)
    #pragma DATA_SECTION(__ccfg, ".ccfg")
    #pragma RETAIN(__ccfg)
    const ccfg_t __ccfg =
    #else
    const ccfg_t __ccfg __attribute__((section(".ccfg"))) __attribute__((used)) =
    #endif
    {
        // Mapped to address
        DEFAULT_CCFG_EXT_LF_CLK,		 // 0x50003FA8 (0x50003xxx maps to last
        DEFAULT_CCFG_MODE_CONF_1,		 // 0x50003FAC  sector in FLASH.
        DEFAULT_CCFG_SIZE_AND_DIS_FLAGS, // 0x50003FB0  Independent of FLASH size)
        DEFAULT_CCFG_MODE_CONF,			 // 0x50003FB4
        DEFAULT_CCFG_VOLT_LOAD_0,		 // 0x50003FB8
        DEFAULT_CCFG_VOLT_LOAD_1,		 // 0x50003FBC
        DEFAULT_CCFG_RTC_OFFSET,		 // 0x50003FC0
        DEFAULT_CCFG_FREQ_OFFSET,		 // 0x50003FC4
        DEFAULT_CCFG_IEEE_MAC_0,		 // 0x50003FC8
        DEFAULT_CCFG_IEEE_MAC_1,		 // 0x50003FCC
        DEFAULT_CCFG_IEEE_BLE_0,		 // 0x50003FD0
        DEFAULT_CCFG_IEEE_BLE_1,		 // 0x50003FD4
        DEFAULT_CCFG_BL_CONFIG,			 // 0x50003FD8
        DEFAULT_CCFG_ERASE_CONF,		 // 0x50003FDC
        DEFAULT_CCFG_CCFG_TI_OPTIONS,	 // 0x50003FE0
        DEFAULT_CCFG_CCFG_TAP_DAP_0,	 // 0x50003FE4
        DEFAULT_CCFG_CCFG_TAP_DAP_1,	 // 0x50003FE8
        DEFAULT_CCFG_IMAGE_VALID_CONF,	 // 0x50003FEC
        DEFAULT_CCFG_CCFG_PROT_31_0,	 // 0x50003FF0
        DEFAULT_CCFG_CCFG_PROT_63_32,	 // 0x50003FF4
        DEFAULT_CCFG_CCFG_PROT_95_64,	 // 0x50003FF8
        DEFAULT_CCFG_CCFG_PROT_127_96,	 // 0x50003FFC
    };
    
    #endif // __CCFC_C__
    

  • Hi Hrishikesh,

    I looked at your CCFG file. For the LF clock, you have selected the option which requires an external oscillator that you don't have in your design. This can explain the issues that you have. CC1310 has an internal RC oscillator that can be used for the LF clock. To select that, please comment out "#define SET_CCFG_MODE_CONF_SCLK_LF_OPTION 0x2 // LF XOSC" on line 186, and uncomment "#define SET_CCFG_MODE_CONF_SCLK_LF_OPTION 0x3        // LF RCOSC" on line 187 in your CCFG file.

    Try this, and please let me know how it went.

    Best regards,

    Haiatullah

  • Dear haiatullah,

    We tried that our end but still we are facing this issue.

    Also i have one query related to this, so even if this was the issue in the CCFG file, but then why it was not showing the same error when we did the touchup to the crystal on our board?

    Regards,

    Hrishikesh.

  • Hi Hrishikesh,

    In that case I will review your design to make sure that there isn't any obvious design fault. In the meantime, I will close this thread.

    Best regards,

    Haiatullah

  • not showing the same error when we did the touchup to the crystal on our board?

    Could you describe what you did here? As far as I see, you have just stated that the soldering is fine (sounding like a visual inspection)

    Has it been double checked that the xtal used is within spec and that the correct load cap is used?

  • Dear TheGhostOf,

    After raising the the first query, we gave the touch up on the crystal still we getting some amount of clock loss issue.

    And we checked the crystal & load capacitor and they looks good.

    Regards,

    Hrishikesh.

     

  • Hi Hrishikesh,

    Do you enter standby any place in your code? Do you use the sleep() function any place in your code?

    Best regards,

    Haiatullah

  • Hello haiatullah,

    Apologies for delayed response.

    yes we have the sleep() functions in our code.

    Regards,

    Hrishikesh.