Other Parts Discussed in Thread: UNIFLASH
I am using BIM and I have write protected the flash with
SET_CCFG_CCFG_TAP_DAP_0_TEST_TAP_ENABLE and SET_CCFG_CCFG_TAP_DAP_0_CPU_DAP_ENABLE
I can unlock the chip with Uniflash for Windows (not linux) but I need a command line tool to unblock it for our build pipeline. I have tried using dslite (windows and linux) with the --mode cc13xx-cc26xx-mass-erase option, but it fails to unlock the chip. The command works OK when the chip is not locked.
Is there a command line method that I can use?
Thanks,
David