Hi Team,
// CMD_FS // Frequency Synthesizer Programming Command rfc_CMD_FS_t RF_cmdFs_slr2500bps2gfsk433mhz_0 = { .commandNo = 0x0803, .status = 0x0000, .pNextOp = 0, .startTime = 0x00000000, .startTrigger.triggerType = 0x0, .startTrigger.bEnaCmd = 0x0, .startTrigger.triggerNo = 0x0, .startTrigger.pastTrig = 0x0, .condition.rule = 0x1, .condition.nSkip = 0x0, .frequency = 0x01BC, .fractFreq = 0x0000, .synthConf.bTxMode = 0x0, .synthConf.refFreq = 0x0, .__dummy0 = 0x00, .__dummy1 = 0x00, .__dummy2 = 0x00, .__dummy3 = 0x0000 };
This paragraph in ti_radio_config.c contains the frequency-related information. If I want to set it dynamically in the code, how should I do it? Is there a step limit for the frequency setting?
Kind regards,
Katherine