I have .xml files for several configurations for the TrxEB board. Using RF Studio, version 2.29, I am loading a .xml file with custom register values and panel values. If I have PKT_CFG1 left as the default value (0x05) and DEV_ADDR left as a default value (0x00) and not specifically changed in the .xml file, and if panel values of 'Address Check, no broadcast' with a Address value of 0x80 are loaded, the registers are not updated. They update, if the user changes them directly. It looks like most imported panel values are not associated with any registers, but a few are. I'm not sure what other possibilities there are. Is that intended, or a bug in the load process?