Hello,
I tried MCUboot example and default is XIP mode.
For mcuboot_blinky example, I have to build 2 FW with different icf base address according to slot offset.
However, we prefer one FW for both slots. In my view, there should be a mapping function implemented by HW to support this.
Please help to confirm if TI support this feature?
primary slot:
/*define symbol __intvec_start__ = 0x8080;
define symbol FLASH_start__ = 0x8080;
define symbol FLASH_end__ = 0x0002ff7f;
define exported symbol MCUBOOT_HDR_BASE = 0x8000;*/
secondary slot:
define symbol __intvec_start__ = 0x3a080;
define symbol FLASH_start__ = 0x3a080;
define symbol FLASH_end__ = 0x0002ff7f;
define exported symbol MCUBOOT_HDR_BASE = 0x3a000;