Other Parts Discussed in Thread: SYSCONFIG
The documentation says the custom RF module in sysconfig allows the user full flexibility in choosing PHY settings but the exact consequences and limitations are not clearly defined.
- What happens in the following scenario?:
- If you use sysconfig to generate phy functions for BLE5 500kbps coded and use those for CMD_BLE5_RADIO_SETUP_PA and CMD_FS, but use together with the CMD_PROP_TX and CMD_PROP_RX commands for transmit and receive, what is the effect of this?
- The coding type is specified in the BLE TX/RX commands, so I’d assume you’re not actually getting coding, is that correct? And, if you’re not actually getting coding, is the true data rate in this setup 1Mbps (becuase 500kbps coding implies two symbol bits per data bit with a symbol rate of 1Msps)?
- If you use sysconfig to generate phy functions for BLE5 500kbps coded and use those for CMD_BLE5_RADIO_SETUP_PA and CMD_FS, but use together with the CMD_PROP_TX and CMD_PROP_RX commands for transmit and receive, what is the effect of this?
- What about the reverse situation? Can the BLE TX/RX commands be used with proprietary radio setup commands, allowing for the use of coding on any proprietary PHY setup?