Other Parts Discussed in Thread: CC1310, , CC1312R
Hi,
I am trying to get WB-DSSS to work with 15.4 stack based projects. So far I was able to integrate radio configurations from SmartRF Studio, and collect/sensor nodes can communicate with each other. I have two questions going forward:
1) Is there a way to sniff WB-DSSS packets? I have tried to use CC1310/1352P launchpads with the latest version of packet sniffer (v1.9), WB-DSSS doesn't seem to be listed as an option in Device Configuration in Sniff Agent. I suppose we can use SmartRF Studio and set it in continuous Packet RX mode. I was able to see quite a few packets this way, but they always have CRC error.
2) How do we setup channel mask? The default 15.4 stack settings uses narrow band, and each channel is only 200KHz apart from adjacent channels.WB-DSSS spreads much wider. Can we continue to use the same scheme for narrow band channels? Or the channel will always be fixed by the radio configurations exported from SmartRF Studio?
Please advise, thanks.
ZL