Other Parts Discussed in Thread: SYSBIOS, SYSCONFIG
/* * File: led_strip.c * * Created on: Aug 8, 2023 * Author: */ #include <stdint.h> #include <stdbool.h> #include <unistd.h> /* POSIX Header files */ #include <semaphore.h> /* Driver Header files */ #include <ti/drivers/GPIO.h> #include <ti/drivers/SPI.h> /* Driver Configuration */ #include <ti/common/cc26xx/uartlog/UartLog.h> #include "ti_drivers_config.h" #define LED_START_FRAME 0x00000000 #define LED_STOP_FRAME 0xFFFFFFFF #define LED_DEFAULT 0xE70FC008 #define LED_OFF 0xE7000000 //RGB #define LED_YELLOW 0x414100E7 #define LED_BLUE 0xE7410000 #define LED_GREEN 0xE7006100 #define LED_RED 0xE7000061 #define LED_STRIP_LEN 5 #define LED_FRAME_SIZE (LED_STRIP_LEN + 2) // 1 - start and 1 -stop frame static SPI_Handle ledSpiHandle; static SPI_Params ledSpiParams; static SPI_Transaction transaction; static bool isCompleted = false; void led_strip_flush_ua_flag(void); void led_strip_off(void); void spiCb(SPI_Handle handle, SPI_Transaction *transaction); void spiCb(SPI_Handle handle, SPI_Transaction *transaction) { if (transaction->status == SPI_TRANSFER_COMPLETED) { isCompleted = true; } } void led_strip_init(void) { SPI_init(); /* Open SPI as controller (default) */ SPI_Params_init(&ledSpiParams); ledSpiParams.frameFormat = SPI_POL0_PHA0; ledSpiParams.mode = SPI_CONTROLLER; /* See device-specific technical reference manual for supported speeds */ ledSpiParams.bitRate = 4000000; ledSpiParams.dataSize = 8; // bit ledSpiParams.transferMode = SPI_MODE_BLOCKING; // ledSpiParams.transferCallbackFxn = spiCb; ledSpiHandle = SPI_open(CONFIG_SPI_1, &ledSpiParams); if (ledSpiHandle == NULL) { Log_error0("SPI handle NULL"); while(1) {}; } } void led_strip_flush_ua_flag(void) { if (ledSpiHandle == NULL) { Log_error0("SPI handle NULL"); while(1) {}; } bool transferOK; uint32_t strip_data[LED_FRAME_SIZE] = {}; // Fill strip strip_data[0] = LED_START_FRAME; for (int i = 1; i <= LED_STRIP_LEN/2; i++) { strip_data[i] = LED_YELLOW; } for (int i = 3; i <= LED_STRIP_LEN; i++) { strip_data[i] = LED_BLUE; } strip_data[LED_FRAME_SIZE-1] = LED_STOP_FRAME; // Init transaction transaction.count = sizeof(strip_data); transaction.txBuf = (void *)strip_data; transaction.rxBuf = (void *)NULL; transferOK = SPI_transfer(ledSpiHandle, &transaction); if (!transferOK) { while(1) {}; } } void led_strip_off(void) { if (ledSpiHandle == NULL) { Log_error0("SPI handle NULL"); while(1) {}; } uint32_t strip_data[LED_FRAME_SIZE] = {}; // Fill strip strip_data[0] = LED_START_FRAME; for (int i = 1; i <= LED_STRIP_LEN; i++) { strip_data[i] = LED_OFF; } strip_data[LED_FRAME_SIZE-1] = LED_STOP_FRAME; // Init transaction transaction.count = sizeof(strip_data); transaction.txBuf = (void *)strip_data; transaction.rxBuf = (void *)NULL; isCompleted = false; bool transferOK = SPI_transfer(ledSpiHandle, &transaction); if (!transferOK) { while(1) {}; } // while (!isCompleted) { //// Task_sleep(10); // } } ///////////////////////////////////////////////////////////// /// USE CASE when it hangs ////////////////////////////////// /// File cr4.cpp void periphInit() { setPinStates(); buttonInit(); setCmdHandlerCb(cmdHandler); led_strip_init(); led_strip_off(); // Hang here sleep(1); flashTest(); } extern "C" Task_Handle* createMainTask() { Task_Params taskParams; // Configure task Task_Params_init(&taskParams); taskParams.stack = sMainTaskStack; taskParams.stackSize = 2048; taskParams.priority = 1; Task_construct(&sMainTask, (ti_sysbios_knl_Task_FuncPtr)mainTask, &taskParams, NULL); sMainTaskHandle = Task_handle(&sMainTask); return &sMainTaskHandle; } /* * ======== mainThread ======== */ void mainTask(void *arg0) { /* Call driver init functions */ periphInit(); m_ext = Extender::getInstance(); while (1) { handleExtInputs(); handleButton(); Task_sleep(10); } }
Hi all! Have an issue with such setup:
CCS Studio Version: 12.6.0.00008
SysConfig: v1.16.2
SimpleLink CC13xx SDK: v7.10.2.23
OS: Ti-RTOS7
Compiler: Clang3.2.1 LTS
Custom-made board
Hardware used:
SPI_1 - used by APA102C led driver (4Leds in series). POCI pin not used, but needed by syscfg
SPI_2 - used by SPI Serial Flash Memory
Used such pins (in SysCfg tool):
#define CONFIG_GPIO_SPI_2_SCLK 28
#define CONFIG_GPIO_SPI_2_POCI 14
#define CONFIG_GPIO_SPI_2_PICO 15
#define CONFIG_GPIO_SPI_1_SCLK 6
#define CONFIG_GPIO_SPI_1_POCI 30
#define CONFIG_GPIO_SPI_1_PICO 5
Syscfg screenshots:
Have problem even when transmitting from SPI_1 in polling, which gives me this fault. When I am changing instances SSI0 to SSI1, one periph (LED in that case) starts to work, but another hangs out on transmit.
Have anyone an example of using 2 separate instances in task context?