Hi,
As the title suggests, I want to make a coap node from the Simplelink Lowpower F2 SDK v7.40 connect with the Silicon Lab's SoC Border Router example, both using FAN 1.1. I've tried changing the certificates on wisun_certificates.h to the same values present under Silicon's Wisun SoC Ping endpoint, however, it seems like both devices aren't even communicating with each other (no change on the led Blink rate). What should I do to make both stacks interoperable?
Thanks in advance,
Thiago