This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
I will be making soon some PCB's with the cc1101 chip and wanted to ask if my layout is ok , or if i can improve some things in my design ? I already made a few PCB with this chip and found the range to be pretty poor , the design was slightly different.
All the components and values are according to the design Specs provided by TI.
info regarding the design:
PCB width = 1mm
Freq = 868 MHZ
antenna = wire
402 components
26mhz Crystal
Here is my new design:8546.Untitled.pdf
And here are some pictures of privios designs :
This is a 868MHZ module , but the range is fare
and this is the 433 MHZ module i made .
Also i think the range could be better :
I would be very happy if some one could tell me what i could improve in my design to get better range:
Best regards Simon Gross
The first thing to do if you suspect that you have poor performance is to measure conducted first. It could be that your schematic/ layout needs improvement but more likely is that your antenna is not 50 ohm.
- Check conducted tx and rx
- Check the antenna impedance
- Ideally you should have added some matching components
Note that the antenna impedance will be very dependent on the surroundings in this case.