I am using the CC1120 in my application where I'm using BFSK with frequency deviation of 9.6kHz, receiver bandwidth of 25kHz and baud rate 1.2kbps. I wanted to evaluate what is the required SNR for CC. To evaluate this I added AWGN noise via the Signal Generator. The settings for noise were 1.92kHz(1.6 times the baud rate as per generators manual) Flat Noise Bandwidth. Error free packets were received at carrier to noise ratio of 9dB. Is this correct or have I made some mistake in the settings? Ideally, what should the required SNR be and what is the accepted method of evaluation of the same?