Hi,
When MODCFG_DEV_E.MOD_FORMAT set to 2-(G)FSK modulation and frequency deviation set to ¼ of symbol rate,it is the MSK modulation.When I use MSK modulation and symbol rate set to 9600,the receive sensitivity reach -114dBm.but when symbol rate is 19200,the receive sensitivity only -108dBm.it is normal taht sensitivity will decrease when symbol rate increase,but if it is too much from -114dBm to -108dBm?And,how to implove receive sensitivity when symbol rate is 19200?
Thanks.