Hi,
I'm running the Beaglebone sensor/gateway example and have it working fine 'stock'.
But, instead of using the UART through the usb (ttyACM0), I want to use the 'real' UART from the CC1350 launchpad connected to ttyS1.
I changed /bin/collector.cfg (changing ttyACM0 to ttyS1) and it works. The problem is that on starting the demo, it says that nothing is connected to ttyACM0. So right now I have to have a 'fake' cc1350 launchpad connected to usb. This 'fake' launchpad is actually programmed as a sensor, while another launchpad is programmed as the coprocessor and connected to ttyS1. Everything works, but I'd like to not have to have anything connected to the usb.
Second, I have multiple gateways running during testing and would like each to have a unique PanID. I changed it from 0xADCD to something else in /bin/collector.cfg, but it seems to not have any effect. The web interface still shows 0xACDC. Likewise, I changed it for the sensors in config.h and they still connect to 0xACDC.
Thanks.