Hi TI team,
I disigned a PCB card with the reccomanded 1W amplifier as the reference said:
I chose with RF Studio the parametrs as noted at the data sheet to get -129dbm sensitiviry (300bps, 1 or 4khz deviation (both tested, 4 is better), 15.6 RX filter).
Nevertheless, I got -120dbm sensitivity (after I checked the attenuators and checked the power of the transmited data).
I use 2 similar boards to test it and a success test is when 50 times the data goes back and forward.
I wonder if you have an idea why I didn't acheive -129dbm (or at least -125..).
thank you!