Other Parts Discussed in Thread: CC113L, TEST2
I have problems with the CC115L transmitter. It lacks power on the output.
I do not have a spectrum analizer to test it, so I do the testing with another CC113L to receive the data and measure RSSI.
With maximum power setting, 0xC0, I can only receive the message form a 1m distance with -90..-95dBm RSSI value.
Now,, I run Linux, so I only use the datasheet to setup the register values and I suspect my problem lies in the reserved register values.
Can anyone help with values from smart-RF for the following reserved registers?
$20, $29..$2B, and the 3 TESTx registers, that also have many reserved bits.
I use it for 433MHz.
Thank you!