Other Parts Discussed in Thread: CC1201
Hi everyOne
I am doing with CC1201, It worked well but with only 920.0Mhz, the Receiver Sensitivity is not good enough, it is about -85dB. At o
static const registerSetting_t preferredSettings[]=
{
{CC1201_IOCFG0, 0x06},
{CC1201_IOCFG2, 0x06},
{CC1201_SYNC_CFG1, 0xA8},//4Bytes 0xA8
{CC1201_SYNC_CFG0, 0x23},
{CC1201_DEVIATION_M, 0x47}, //Deviation 12.5kHz:0x47
{CC1201_MODCFG_DEV_E, 0x0A},//2-GFSK
{CC1201_DCFILT_CFG, 0x4B},
{CC1201_PREAMBLE_CFG1, 0x19},//4Bytes Preamble 0x55
{CC1201_PREAMBLE_CFG0, 0x8A},
{CC1201_IQIC, 0xD8},
{CC1201_CHAN_BW, 0x21}, //DC Filter BW 50>0x21
{CC1201_MDMCFG1, 0x42},
{CC1201_MDMCFG0, 0x05},
{CC1201_SYMBOL_RATE2, 0x84},//25kbps 0x84
{CC1201_SYMBOL_RATE1, 0x7A},// 0x7A
{CC1201_SYMBOL_RATE0, 0xE1},// 0xE1
{CC1201_AGC_REF, 0x24},
{CC1201_AGC_CS_THR, 0x01},
{CC1201_AGC_GAIN_ADJUST, 0xB0},//offset of RSSI -80dB 0xB0
{CC1201_AGC_CFG1, 0x12},
{CC1201_AGC_CFG0, 0x80},
{CC1201_FIFO_CFG, 0x00},
{CC1201_FS_CFG, 0x12},
{CC1201_PKT_CFG2, 0x00},
{CC1201_PKT_CFG1, 0x01},//No use CRC on hardware
//Follow after data byte will be RSSI byte, and CRC_NG bit, LQI (7bit),
{CC1201_RFEND_CFG0, 0x30},//After transfer will automatically change to receiver
{CC1201_RFEND_CFG1, 0x3E},//After receiver will automatically change to receiver
{CC1201_PA_CFG1, 0x3F},//PA_CFG1bit5:0
{CC1201_PKT_LEN, 0x09},//fixed 9 bytes
{CC1201_IF_MIX_CFG, 0x1C},
{CC1201_TOC_CFG, 0x03},
{CC1201_MDMCFG2, 0x02},
{CC1201_FREQ2, 0x5C}, //920.0Mhz
{CC1201_FREQ1, 0x00}, //920.0Mhz
{CC1201_FREQ0, 0x00}, //920.0Mhz
{CC1201_IF_ADC1, 0xEE},
{CC1201_IF_ADC0, 0x10},
{CC1201_FS_DIG1, 0x04},
{CC1201_FS_DIG0, 0x55},
{CC1201_FS_CAL1, 0x40},
{CC1201_FS_CAL0, 0x0E},
{CC1201_FS_DIVTWO, 0x03},
{CC1201_FS_DSM0, 0x33},
{CC1201_FS_DVC0, 0x17},
{CC1201_FS_PFD, 0x00},
{CC1201_FS_PRE, 0x6E},
{CC1201_FS_REG_DIV_CML, 0x1C},
{CC1201_FS_SPARE, 0xAC},
{CC1201_FS_VCO0, 0xB5},
{CC1201_IFAMP, 0x09},
{CC1201_XOSC5, 0x0E},
{CC1201_XOSC1, 0x03},
{CC1201_PARTNUMBER, 0x21},
{CC1201_PARTVERSION, 0x11},
{CC1201_MODEM_STATUS1, 0x10},
};
I checked with 915.25/919.75/920.25/920.6 Mhz, the Receiver Sensitivity is 100dB.
I used almost setting from SmartRF. I include setting parameter on txt file , If someOne did or pretend to do with 920Mhz, please share the result.
On this Txt file i use 4bytes preamble, 4 bytes synwords, 9 bytes fixed data length, disable CRC, 2GFSK, 25kbps, 12.5khz Deviation, RXFilterBW 50khz.
By anyway, thanks for your interest.