This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CC1120DK
Hello.
We have the CC1120DK.
We try to test the modules like in the TI video(www.youtube.com/watch, but at the Master I can't run PER STATISTICS and plot the connection because I do not have menu like that.
At start, under Main Menu also we have 5 submenus different like in your video:
1.PER Test
2.Easy Link Test
3.RX Sniff Test
4.Chip Information
5.Set Contrast
Also at Linking device Master says "Device linking failed" but the Slave meanwhile says "Test Running" I do not know if it is OK or NOT.
At device start it is written v4.3 .From Smart RF Studio 7 I updated but nothing changed.
Can you help please?
Thank you for reply.
I chose USB Mode:Enable and Smart RF.
This way I see the EM in Smart RF Studio 7, but I could not link the two EM devices this way via Radio Frequency.
I could link the two EM devices only in UART Mode, but at the Master side tells "Linking failed", but they are linked because the Slave tells "Test Running".After This I cant plot at EB display the PER Statistics, because I have no such menu.
I could not reflash the TrxEB.I read the EB User Guide Firmware Update part.I downloaded Smart RF Programmer 2 and connected MSP with EB and started Smart RF Programmer, but did not recognise the EB.
Can you help with steps?