Hello.
I've got two TrxEB development board with a 868 MHz radio. One of the boards will not detect a inserted radio chip. The LED above the enable/disable switch i just blinking. When i connect to the SmartRF Studio app the TrxEB board is detected but claims that no chip is present. But when i switch the radio board from one board to the other the error is the same, so the problem must be with the TrxEB board.
Is there a way to fix/reset this error? Or do i need a new board?
Regards
Henrik