This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC1352R1: How to use external antennas with CC1352R launchpad

Part Number: LAUNCHXL-CC1352R1
Other Parts Discussed in Thread: CC-ANTENNA-DK2

Hi,

I am currently developing a project using the LAUNCHXL-CC1352R1 and I recently realized that the external antenna connections are not completed in the launchpad. As I see it, I would have to unmount R16 and mount R19 and unmount C36 and mount C37 in order to use the JSC connections instead of the PCB antenna. If I want to use the SMA I would have to unmount C482 and mount C483. 

Is this information correct? What are the values of these components that should be mounted in the launchpad? Do they have the same values of the components I would have to unmount in order to mount them? Any information about the launchpad and its connections to external antennas would be very useful.

My plan is to use the Sub-1GHz with an external antenna coming from the CC-Antenna-DK2 kit. 

Thanks in advance for the help.