This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDC-01002: Can't open network

Part Number: TIDC-01002
Other Parts Discussed in Thread: CC3220SF, UNIFLASH

Hi

I am experiencing the exaxt same problems as in the question this thread is related to:

- the "open" button on the cloud app is only visible for a very brief moment

- nothing happens when I click on the reset button of the MAC-CoP

This is what I have:

- I used the prebuild images from the current master branch of the TIDC-01002 git repo

- I have provisioned the CC3220SF and I can connect to the cloud. This is also shown in the Watson Device Dashboard

- I have two CC1352P1 boards. I flashed "CC13x2_LaunchPad/coprocessor_cc1352lp.hex" to the MAC-CoP and sensor_cc13x2_lp_default_863.hex to the Sensor board.

- I changed the jumpers on the MAC-CoP board according to the doc and MAC-CoP board is stacked on the CC3220SF , only one power supply micro USB to the CC3220SF. No Leds are on on the MAC-CoP

- the MAC-CoP board has been previously used with Project 0 as a collector node and is know to operate.

- all UNIFLASH 5.1.0.2397 flash actions concluded without errors

- Linux Mint 19.2

Kind regards

Peter