Other Parts Discussed in Thread: ENERGYTRACE
Tool/software: Code Composer Studio
After my complain about the not working EnergyTrace in CCS9.2 i've got the answer that the problem is solved with CCS9.3. But it is not solved. It is still not working.
If i start EnergyTrace while in debug-mode i get a bunch of errormessages in the console window :
Cortex_M4_0: GEL Output: Memory Map Initialization Complete.
Cortex_M4_0: GEL Output: Board Reset Complete.
IcePick_C: Error: (Error -261 @ 0xFFFFFEFB) Invalid response was received from the XDS110. (Emulation package 9.1.0.00001)
CS_DAP_0: Error: (Error -261 @ 0x0) Invalid response was received from the XDS110. (Emulation package 9.1.0.00001)
IcePick_C: Error: (Error -261 @ 0xFFFFFEFB) Invalid response was received from the XDS110. (Emulation package 9.1.0.00001)
IcePick_C: Error: (Error -261 @ 0xFFFFFEFB) Invalid response was received from the XDS110. (Emulation package 9.1.0.00001)
IcePick_C: Error: (Error -261 @ 0xFFFFFEFB) Invalid response was received from the XDS110. (Emulation package 9.1.0.00001)
Beside this i get unrealistic values: Peak-Current 120mA with all task are sleeping and wait for some HW-events.
And if i try to start EnergyTrace in Stand-alone-mode, it doesn't start. It shows a progress window with 'Detecting EnergyTrace Pod' and after a short time the window disappears and nothing more happens.