Hello,
Does the Simplelink CC13x0 SDK 4.10.00.10 support the Security Manager (SM) module? I have attempted to enable Secure Commissioning on my sensor example's features.h file but I get the following linking error:
<Linking> error: symbol "macWrapperAddKeyInitFCtr" redeclared with incompatible type: "uint8(ApiMac_secAddKeyInitFrameCounter_t *)[unsigned char [ExplSign] ]" in "../Application/MAC/HighLevel/mac_hl_patch.c" at line 1156 and: "uint8(ApiMac_secAddKeyInitFrameCounter_t *)[unsigned char [ExplSign] ]" in ".../ti154stack/high_level/macwrapper.h" at line 185) error: symbol "macWrapperAddDevice" redeclared with incompatible type: "uint8(ApiMac_secAddDevice_t *)[unsigned char [ExplSign] ]" in "../Application/MAC/HighLevel/mac_hl_patch.c" at line 1460 and: "uint8(ApiMac_secAddDevice_t *)[unsigned char [ExplSign] ]" in ".../ti154stack/high_level/macwrapper.h" at line 95)
I know it is supported for the CC13x2 SDK, and since the code is also provided on the CC13x0 version I thought maybe it could work as well, but I am not sure if maclib_secure_cc13x0.a is prepared for it yet. Thank you for your time.
Kind regards,
Ricardo Cirio