Other Parts Discussed in Thread: CC3235MODSF, CC3235MODS, UNIFLASH
Hi experts,
My customer is considering using both CC3235MODS and CC3235MODSF to avoid supply side risks.
Q1: Is the following correct about how to use the built-in Flash in the two devices?
CC3235MODS・・・Stores application image in 4Mbyte sFlash. extracts to SRAM and then executes the image.
CC3235MODSF・・・Stores application image in a 4 Mbyte sFlash, copies it to a 1 Mbyte XIP Flash, and then executes the image. Or, extract to SRAM and then execute the image.
Q2: Can I use the same method to write the application image in these two?
Am I correct in understanding that we can write to the sFlash built into both of them in the same way through Uniflash?
Q3: Is it possible to identify these two types of devices when communicating from the outside?
It seems that there is no Device Descriptors (TLV) area in ROM.
Q4: If SPI Flash is used externally, is it correct to recognize that SPI Flash is not allocated to the memory map?
We are inexperienced with CC32xxMOD products, so we would appreciate your help.
Best regards,
O.H