Hi,
hi try to use Triggered roaming :
SlWlanNetworkAssistedRoaming_t roamingTriggeringEnable;
roamingTriggeringEnable.Enable = 1;
roamingTriggeringEnable.rssiThreshold = -63;
sl_WlanSet(SL_WLAN_STA_NETWORK_ASSISTED_ROAMING, SL_WLAN_ROAMING_TRIGGERING_ENABLE, sizeof(SlWlanNetworkAssistedRoaming_t ), (_u8 *)&roamingTriggeringEnable );
1. can you tell me if the function "Triggered roaming" retains its settings when the module is switched off ?
2. does it work with all connections policy?
3. Is it possible to know in which SL_WLAN_STA_NETWORK_ASSISTED_ROAMING the module currently is?
Thx
Maxime