This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WL1835MOD: wl18xx firmware and configuration file

Part Number: WL1835MOD


Just as a confirmation, below is what I have used in my project. Please confirm all the steps below are ok:

 

I intend to use latest WiLink firmware for WiFi and BT. So I downloaded wl18xx-fw-4.bin version 8.9.0.0.90 from the below link:

https://git.ti.com/cgit/wilink8-wlan/wl18xx_fw/tree/?id=6c5ca87b9a912f09d090d5e1b6ace86d26718888

For using this version of firmware, as per the documentation, I had to run the configure-device.sh script. (this is ok?) This is how I run it:

  1. Copy the contents of the latest 18xx-ti-utils-master/wlconf folder into /usr/sbin/wlconf (I got 18xx-ti-utils from this https://git.ti.com/cgit/wilink8-wlan/18xx-ti-utils/ master branch)
  2. Run the command ./configure_device.sh
    1. Using TI module: Yes
    2. Chip flavor: WL1835MODGB so I gave 1835
    3. Number of 2.4GHz antennas fitted: 2
  3. After doing that, I got wl18xx-conf.bin in /lib/firmware/ti-connectivity/               folder
  4. This file wl18xx-conf.bin along with the wl18xx-fw-4.bin is to be used at our end I suppose. When I compare this wl18xx-conf.bin with my current file, I see a lot of differences. Please confirm these differences are expected and are ok. Attached are the two files: wl18xx_original, wl18xx_new (generated today based on the above instructions).

 Latest BLE firmware: 11.8.32

https://git.ti.com/cgit/ti-bt/service-packs/commit/?id=3aa1d75f3c2ae77f6e4d36194e3d281b899ab149