Hi,
I think I have a problem with wl18xx problem
I am using beaglebone blue
[53233.855249] wlcore: ERROR SW watchdog interrupt received! starting recovery.
[53233.862422] ------------[ cut here ]------------
[53233.862728] WARNING: CPU: 0 PID: 1231 at drivers/net/wireless/ti/wlcore/main. c:808 wl12xx_queue_recovery_work+0x64/0x68 [wlcore]
[53233.862737] Modules linked in: usb_f_acm u_serial usb_f_ecm aes_arm_bs crypto _simd cryptd usb_f_mass_storage usb_f_rndis u_ether libcomposite xt_state xt_con ntrack nft_counter nft_chain_nat_ipv4 ipt_MASQUERADE nft_compat wl18xx wlcore ma c80211 rfcomm cfg80211 bnep pm33xx wkup_m3_rproc wkup_m3_ipc hci_uart btqca btbc m btintel bluetooth ch341 ecdh_generic usbserial wlcore_sdio uio_pdrv_genirq uio pruss_soc_bus pru_rproc pruss irq_pruss_intc remoteproc virtio virtio_ring spid ev
[53233.862850] CPU: 0 PID: 1231 Comm: irq/156-wl18xx Tainted: G W 4.19.94-ti-r73 #1buster
[53233.862856] Hardware name: Generic AM33XX (Flattened Device Tree)
[53233.862900] [<c0113e18>] (unwind_backtrace) from [<c010e388>] (show_stack+0x2 0/0x24)
[53233.862920] [<c010e388>] (show_stack) from [<c0d2909c>] (dump_stack+0x8c/0xa0 )
[53233.862938] [<c0d2909c>] (dump_stack) from [<c013c928>] (__warn.part.3+0xcc/0 xe8)
[53233.862951] [<c013c928>] (__warn.part.3) from [<c013cac4>] (warn_slowpath_nul l+0x54/0x5c)
[53233.863086] [<c013cac4>] (warn_slowpath_null) from [<bf3b3cb0>] (wl12xx_queue _recovery_work+0x64/0x68 [wlcore])
[53233.863270] [<bf3b3cb0>] (wl12xx_queue_recovery_work [wlcore]) from [<bf3b449 8>] (wlcore_irq+0x118/0x188 [wlcore])
[53233.863375] [<bf3b4498>] (wlcore_irq [wlcore]) from [<c01afe1c>] (irq_thread_ fn+0x2c/0x88)
[53233.863389] [<c01afe1c>] (irq_thread_fn) from [<c01b0194>] (irq_thread+0x164/ 0x234)
[53233.863402] [<c01b0194>] (irq_thread) from [<c01604c0>] (kthread+0x16c/0x174)
[53233.863416] [<c01604c0>] (kthread) from [<c01010e8>] (ret_from_fork+0x14/0x2c )
[53233.863424] Exception stack(0xdb131fb0 to 0xdb131ff8)
[53233.863436] 1fa0: 00000000 00000000 00000 000 00000000
[53233.863446] 1fc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000 000 00000000
[53233.863456] 1fe0: 00000000 00000000 00000000 00000000 00000013 00000000
[53233.863465] ---[ end trace 9705a47acaa13116 ]---
[53233.863641] wlcore: Hardware recovery in progress. FW ver: Rev 8.9.0.0.88
[53233.864322] wlcore: pc: 0xf406, hint_sts: 0x00000000 count: 1
[53233.864795] wlcore: down
[53233.864846] wlcore: down
[53233.864873] wlcore: down
[53233.865032] ieee80211 phy0: Hardware restart was requested
[53234.281108] wlcore: PHY firmware version: Rev 8.2.0.0.245
[53234.330059] wlcore: firmware booted (Rev 8.9.0.0.88)
[53234.366255] wlcore: Association completed.
[53271.818887] wlan0: deauthenticated from a2:b5:3c:0c:cd:02 (Reason: 1=UNSPECIF IED)
[53271.974546] IPv6: ADDRCONF(NETDEV_UP): wlan0: link is not ready
[53271.990792] IPv6: ADDRCONF(NETDEV_UP): wlan0: link is not ready
[53272.676460] wlan0: authenticate with a2:b5:3c:0c:cd:02
[53272.694436] wlan0: send auth to a2:b5:3c:0c:cd:02 (try 1/3)
[53272.798353] wlan0: authenticated
[53272.805665] wlan0: associate with a2:b5:3c:0c:cd:02 (try 1/3)
[53272.810630] wlan0: RX AssocResp from a2:b5:3c:0c:cd:02 (capab=0x1411 status=0 aid=11)
[53272.840036] wlan0: associated
[53272.845805] wlan0: Limiting TX power to 20 (20 - 0) dBm as advertised by a2:b 5:3c:0c:cd:02
[53273.890556] IPv6: ADDRCONF(NETDEV_CHANGE): wlan0: link becomes ready
[53273.926356] wlcore: Association completed.
[58147.954725] wlcore: ERROR SW watchdog interrupt received! starting recovery.